NXOpen.UF.Sf.MeshVisuals Structure¶
NXOpen.UF.Sf.MeshVisuals is an alias for NXOpen.UF.SfMeshVisuals_Struct
-
class
NXOpen.UF.
SfMeshVisuals_Struct
¶ Bases:
object
Refer to UF_SF_mesh_visuals_s for documentation.
Fields
NXOpen.UF.SfMeshVisuals_Struct.Color |
Primary element color |
NXOpen.UF.SfMeshVisuals_Struct.ShadeMode |
Different modes of shading: 0 - never shade 1 - shade when any shade mode is on 2 - shade when partial shaded mode is on 3 - shade when fully shaded mode is on |
NXOpen.UF.SfMeshVisuals_Struct.ShadeEdgeColor |
Element edge color when shaded |
NXOpen.UF.SfMeshVisuals_Struct.ShrinkFactor |
Element shrink percentage 0 -> 100 0 - no shrinking 100 - shrinks elements to a point |
NXOpen.UF.SfMeshVisuals_Struct.Normals |
Valid for 2D elements 0 - no element normals 1 - element directional tails 2 - element vectors |
NXOpen.UF.SfMeshVisuals_Struct.NormalsColor |
Normal display color |
NXOpen.UF.SfMeshVisuals_Struct.EdgeVisibilitySw |
Element edge visibility switch: 0 - do not show elemement edges 1 - show element edges |
NXOpen.UF.SfMeshVisuals_Struct.TextDisplaySw |
Element text display switch: 0 - do not show text 1 - show text |
NXOpen.UF.SfMeshVisuals_Struct.ThickShellSw |
Element thick shell display switch: 0 - do not show 2D elements as thick shells 1 - show 2D elements as thick shells |
NXOpen.UF.SfMeshVisuals_Struct.ShowAnalysis |
Show analysis results or not * 0 - do not show analysis results * 1 - show analysis results |
NXOpen.UF.SfMeshVisuals_Struct.ShowDeformed |
Show deformation or not . |
NXOpen.UF.SfMeshVisuals_Struct.DeformedScale |
Scale value for the deformation magnitude * if show deformation is requested |