NXOpen.UF.Sflegend.Attr Structure¶
NXOpen.UF.Sflegend.Attr is an alias for NXOpen.UF.SfLegendAttr_Struct
Fields
NXOpen.UF.SfLegendAttr_Struct.AttrMask |
This field is set to one or more of the following symbols OR’d together to indicate which of the remaining fields of the structure are set. |
NXOpen.UF.SfLegendAttr_Struct.WidthPercent |
The percentage of the display which the legend occupies. |
NXOpen.UF.SfLegendAttr_Struct.BorderSw |
Switch indicating whether or not the border of the legend gets displayed. |
NXOpen.UF.SfLegendAttr_Struct.FontSize |
The size in inches of an individual character. |
NXOpen.UF.SfLegendAttr_Struct.FontColor |
font color |
NXOpen.UF.SfLegendAttr_Struct.Header |
The header text of the legend area default: none defined. |
NXOpen.UF.SfLegendAttr_Struct.IndexAttr |
The index area’s attributes if defined. |
NXOpen.UF.SfLegendAttr_Struct.Footer |
The footer text of the legend area default: none defined. |
NXOpen.UF.SfLegendAttr_Struct.LayoutType |
|
NXOpen.UF.SfLegendAttr_Struct.ViewPortId |
viewport |