NXOpen.UF.Sf.ContactMeshData Structure¶
NXOpen.UF.Sf.ContactMeshData is an alias for NXOpen.UF.SfContactMeshData_Struct
-
class
NXOpen.UF.
SfContactMeshData_Struct
¶ Bases:
object
Refer to UF_SF_contact_mesh_data_s for documentation.
Fields
NXOpen.UF.SfContactMeshData_Struct.ElementName |
refer to uf_sf_lang_names.h |
NXOpen.UF.SfContactMeshData_Struct.ElementDescritorTag |
Set it to NULL_TAG |
NXOpen.UF.SfContactMeshData_Struct.AlignTargetEdgeNode |
0 - Equal Distance 1 - Minimum Distance or Normal To |
NXOpen.UF.SfContactMeshData_Struct.TargetEdgeNodeAlignMethod |
0 - Minimum Distance 1 - Normal To |
NXOpen.UF.SfContactMeshData_Struct.NumberOfElms |
required |
NXOpen.UF.SfContactMeshData_Struct.GapTolOption |
0 - Do not apply tol 1 - Apply gap tolerance |
NXOpen.UF.SfContactMeshData_Struct.GapTolerance |
Gap tolerance option 0: Don’t apply tolerance 1: Apply tolerance |
NXOpen.UF.SfContactMeshData_Struct.ContactEdge |
Tag of the contact edge. |
NXOpen.UF.SfContactMeshData_Struct.ContactEdgeMeshDir |
Direction of the mesh for the contact edge: UF_SF_MG_MESHDIR_FROM_START UF_SF_MG_MESHDIR_FROM_END |
NXOpen.UF.SfContactMeshData_Struct.ContactEdgeStartLimit |
Limit of edge starting for the contact edge. |
NXOpen.UF.SfContactMeshData_Struct.ContactEdgeEndLimit |
Limit of edge ending for the contact edge. |
NXOpen.UF.SfContactMeshData_Struct.TargetEdge |
Tag of the target edge. |
NXOpen.UF.SfContactMeshData_Struct.TargetEdgeMeshDir |
Direction of the mesh for the target edge: UF_SF_MG_MESHDIR_FROM_START UF_SF_MG_MESHDIR_FROM_END |
NXOpen.UF.SfContactMeshData_Struct.TargetEdgeStartLimit |
set start limits to 0 and end limits to 1 to build contact mesh between entire length of the edges. |
NXOpen.UF.SfContactMeshData_Struct.TargetEdgeEndLimit |
Limit of edge ending for the target edge. |