NXOpen.UF.Scop.VectorData Structure

NXOpen.UF.Scop.VectorData is an alias for NXOpen.UF.ScopVectorData_Struct

class NXOpen.UF.ScopVectorData_Struct

Bases: object

Refer to UF_SCOP_vector_data_s for documentation.

Fields

NXOpen.UF.ScopVectorData_Struct.Xyz the vector location
NXOpen.UF.ScopVectorData_Struct.Ijk the vector direction, if data type is UF_SCOP_TX_INTP_DATYPE_VECTOR
NXOpen.UF.ScopVectorData_Struct.LeadTilt the vector lead angle and tilt angle, if data type is UF_SCOP_TX_INTP_DATYPE_ANGLE_DS or UF_SCOP_TX_INTP_DATYPE_ANGLE_PS
NXOpen.UF.ScopVectorData_Struct.IsCornerVector If TRUE, this vector can not be deleted.