NXOpen.UF.Plist.Prefs Structure¶
NXOpen.UF.Plist.Prefs is an alias for NXOpen.UF.PlistPrefs_Struct
-
class
NXOpen.UF.
PlistPrefs_Struct
¶ Bases:
object
Refer to UF_PLIST_prefs_s for documentation.
Fields
NXOpen.UF.PlistPrefs_Struct.SectionPrefs |
Preferences used for creating new sections |
NXOpen.UF.PlistPrefs_Struct.GrowDirection |
Does the parts list grow upward or downward? |
NXOpen.UF.PlistPrefs_Struct.LdrMethod |
Method used to show rows that are both locked and deleted |
NXOpen.UF.PlistPrefs_Struct.CreateNewRowsAsLocked |
Should newly created rows automatically be locked? |
NXOpen.UF.PlistPrefs_Struct.InitialCalloutField |
String used for the first callout in the parts list. |
NXOpen.UF.PlistPrefs_Struct.CalloutIncrement |
Value by which the callout increments |
NXOpen.UF.PlistPrefs_Struct.SymbolType |
Type of object used for auto creation and placement of callout symbols |
NXOpen.UF.PlistPrefs_Struct.MainSymbolText |
Format of the string used in the main callout symbol This string can contains automatic text control sequences as follows: $= - Auto Member - Expands to the name of the member $~C - Auto Callout - Expands to the value of the callout $~Q - Auto Quantity - Expands to the value of the first non-zero quantity field |
NXOpen.UF.PlistPrefs_Struct.RefSymbolText |
Format of the string used in the reference callout symbol This is in the same format as main_symbol_text |
NXOpen.UF.PlistPrefs_Struct.CharactersToSkip |
List of callout chars to skip |
NXOpen.UF.PlistPrefs_Struct.AutoUpdate |
Should the parts list automatically update when the model changes? |
NXOpen.UF.PlistPrefs_Struct.SortOnUpdate |
Should a sort be done during update? |
NXOpen.UF.PlistPrefs_Struct.HighlightManualText |
Should manual text be hilited? |
NXOpen.UF.PlistPrefs_Struct.Isprotected |
Should parts list be protected ? |
NXOpen.UF.PlistPrefs_Struct.Allowmanualrows |
Are parts list allow manual row insertion? |