NXOpen.UF.Pd.AttributeValue Structure¶
NXOpen.UF.Pd.AttributeValue is an alias for NXOpen.UF.PdAttributeValue_Struct
-
class
NXOpen.UF.
PdAttributeValue_Struct
¶ Bases:
object
Refer to UF_PD_attribute_value_s for documentation.
Fields
NXOpen.UF.PdAttributeValue_Struct.ValueType |
Type of attribute value (string, int, etc.) |
NXOpen.UF.PdAttributeValue_Struct.ValueTitle |
Title of the product attributes value, * the valid value titles are defined in each product * attribute, refer UF_PD_attribute_type_e |
NXOpen.UF.PdAttributeValue_Struct.IntegerValue |
Integer value of the attribute coresponding to the value_type |
NXOpen.UF.PdAttributeValue_Struct.NumberValue |
Number value of the attribute coresponding to the value_type |
NXOpen.UF.PdAttributeValue_Struct.StringValue |
String value/list value of the attribute coresponding to the value_type |