NXOpen.UF.Path.ToolChange Structure¶
NXOpen.UF.Path.ToolChange is an alias for NXOpen.UF.PathToolChange_Struct
-
class
NXOpen.UF.
PathToolChange_Struct
¶ Bases:
object
Refer to UF_PATH_tool_change_s for documentation.
Fields
NXOpen.UF.PathToolChange_Struct.XoffsetValue |
offset value of the tool in the X direction. |
NXOpen.UF.PathToolChange_Struct.YoffsetValue |
offset value of the tool in the Y direction. |
NXOpen.UF.PathToolChange_Struct.ZoffsetValue |
offset value of the tool in the Z direction. This value is only used by mill. |
NXOpen.UF.PathToolChange_Struct.ToolAngle |
the angle at which the tool is mounted. |
NXOpen.UF.PathToolChange_Struct.Radius |
the nose radius of the tool |
NXOpen.UF.PathToolChange_Struct.ToolNumber |
The tool number |
NXOpen.UF.PathToolChange_Struct.AdjustRegister |
the register to use for tool length compensation |
NXOpen.UF.PathToolChange_Struct.HeadType |
The type of the head. |
NXOpen.UF.PathToolChange_Struct.AdjustFlag |
the adjust register is output if and only if this is TRUE. |
NXOpen.UF.PathToolChange_Struct.ToolOffsetFlag |
the tool offsets are output if and only if this is TRUE. |
NXOpen.UF.PathToolChange_Struct.ToolNumberFlag |
the tool number is output if and only if this is TRUE. |
NXOpen.UF.PathToolChange_Struct.ToolAngleRadiusFlag |
the tool angle and radius are output if and only if this TRUE |
NXOpen.UF.PathToolChange_Struct.ManualChangeFlag |
the string MANUAL is output if and only if this is TRUE. |