NXOpen.UF.Path.HelicalMotion Structure¶
NXOpen.UF.Path.HelicalMotion is an alias for NXOpen.UF.PathHelicalMotion_Struct
-
class
NXOpen.UF.
PathHelicalMotion_Struct
¶ Bases:
object
Refer to UF_PATH_helical_motion_s for documentation.
Fields
NXOpen.UF.PathHelicalMotion_Struct.Start |
this array specifies the start point x,y,z coordinates(this should be the end point of the previous motion) |
NXOpen.UF.PathHelicalMotion_Struct.StartToolAxis |
This array specifies the starting tool axis. |
NXOpen.UF.PathHelicalMotion_Struct.End |
this array specifies the end point x,y,z coordinates. |
NXOpen.UF.PathHelicalMotion_Struct.EndToolAxis |
This array specifies the ending tool axis. |
NXOpen.UF.PathHelicalMotion_Struct.ArcAxis |
this array specifies the vector which is the axis of the motion. |
NXOpen.UF.PathHelicalMotion_Struct.ArcCenter |
this array specifies the x,y,z coordinates of the center of the helix at the end point. |
NXOpen.UF.PathHelicalMotion_Struct.ArcRadius |
This is the radius of the helix. |
NXOpen.UF.PathHelicalMotion_Struct.Tolerance |
Tolerance to be used for arc fits. |
NXOpen.UF.PathHelicalMotion_Struct.Times |
Number of Turns including partial turn |
NXOpen.UF.PathHelicalMotion_Struct.FeedValue |
This is the feed rate value. |
NXOpen.UF.PathHelicalMotion_Struct.FeedUnit |
This specifies the units of the feed value. |
NXOpen.UF.PathHelicalMotion_Struct.Type |
This is the type of the motion. |
NXOpen.UF.PathHelicalMotion_Struct.MaterialSide |
This specifies the material side. |
NXOpen.UF.PathHelicalMotion_Struct.Shape |
This specifies the shape. |