NXOpen.UF.Part.LoadStatus Structure¶
NXOpen.UF.Part.LoadStatus is an alias for NXOpen.UF.PartLoadStatus_Struct
-
class
NXOpen.UF.
PartLoadStatus_Struct
¶ Bases:
object
Refer to UF_PART_load_status_s for documentation.
Fields
NXOpen.UF.PartLoadStatus_Struct.Failed |
Output: True if the load failed and was rolled back |
NXOpen.UF.PartLoadStatus_Struct.UserAbort |
Output: True if the only ‘failure’ was user abort |
NXOpen.UF.PartLoadStatus_Struct.NParts |
Output: Length of the following two allocated arrays. |
NXOpen.UF.PartLoadStatus_Struct.FileNames |
Allocated array of file names |
NXOpen.UF.PartLoadStatus_Struct.Statuses |
Allocated array of associated status codes for each file name. |