NXOpen.UF.Param.IndexAttribute Structure¶
NXOpen.UF.Param.IndexAttribute is an alias for NXOpen.UF.ParamIndexAttribute_Struct
-
class
NXOpen.UF.
ParamIndexAttribute_Struct
¶ Bases:
object
Refer to UF_PARAM_index_attribute_s for documentation.
Fields
NXOpen.UF.ParamIndexAttribute_Struct.Key |
The unique integer for this parameter |
NXOpen.UF.ParamIndexAttribute_Struct.Name |
The parameter’sname |
NXOpen.UF.ParamIndexAttribute_Struct.Type |
See UF_PARAM_type_t definition |
NXOpen.UF.ParamIndexAttribute_Struct.IntDefault |
If type is integer then its default value |
NXOpen.UF.ParamIndexAttribute_Struct.DblDefault |
If type is double then its default value |
NXOpen.UF.ParamIndexAttribute_Struct.RegenFlag |
What to regenerate if parameter changes |