NXOpen.UF.Obj.DispProps Structure¶
NXOpen.UF.Obj.DispProps is an alias for NXOpen.UF.ObjDispProps_Struct
-
class
NXOpen.UF.
ObjDispProps_Struct
¶ Bases:
object
Refer to UF_OBJ_disp_props_s for documentation.
Fields
NXOpen.UF.ObjDispProps_Struct.Layer |
the layer an object resides on |
NXOpen.UF.ObjDispProps_Struct.Color |
the color an object possesses |
NXOpen.UF.ObjDispProps_Struct.BlankStatus |
the blank status of an object This status is defined by one of the two string defined constants: UF_OBJ_NOT_BLANKED UF_OBJ_BLANKED |
NXOpen.UF.ObjDispProps_Struct.LineWidth |
the line width of an object Can be one of the following : UF_OBJ_WIDTH_NORMAL UF_OBJ_WIDTH_THICK UF_OBJ_WIDTH_THIN UF_OBJ_WIDTH_ORIGINAL UF_OBJ_WIDTH_1 – UF_OBJ_WIDTH_9 |
NXOpen.UF.ObjDispProps_Struct.Font |
the font an object possesses |
NXOpen.UF.ObjDispProps_Struct.HighlightStatus |
the highlight status of an object where TRUE indicates that highlight is on. |