NXOpen.UF.Motion.SpringDamper Structure¶
NXOpen.UF.Motion.SpringDamper is an alias for NXOpen.UF.MotionSpringDamper_Struct
-
class
NXOpen.UF.
MotionSpringDamper_Struct
¶ Bases:
object
Refer to UF_MOTION_spring_damper_s for documentation.
Fields
NXOpen.UF.MotionSpringDamper_Struct.Name |
The name of the spring damper. |
NXOpen.UF.MotionSpringDamper_Struct.SprDmpType |
The type of spring/damper. |
NXOpen.UF.MotionSpringDamper_Struct.Joint |
The joint owning the spring/damper if the spring/damper type is UF_MOTION_revolute_spring_damper or UF_MOTION_slider_spring_damper. |
NXOpen.UF.MotionSpringDamper_Struct.Link1 |
Link one of the spring/damper if the spring/damper type is UF_MOTION_link_spring_damper. |
NXOpen.UF.MotionSpringDamper_Struct.Point1 |
The point of the spring/damper attachment on the first link. |
NXOpen.UF.MotionSpringDamper_Struct.Pt1Coord |
The coordinates of the attachment point of the spring/damper on the first link. |
NXOpen.UF.MotionSpringDamper_Struct.Link2 |
Link two of the spring/damper, or NULL_TAG if ground. |
NXOpen.UF.MotionSpringDamper_Struct.Point2 |
The point of the spring/damper attachment on the second link, or the point of attachment to ground if link_2 is NULL_TAG. |
NXOpen.UF.MotionSpringDamper_Struct.Pt2Coord |
The coordinates of the attachment point of the spring/damper to the second link, or to ground. |
NXOpen.UF.MotionSpringDamper_Struct.SpringRate |
The spring rate for both rotational and translational springs. |
NXOpen.UF.MotionSpringDamper_Struct.SpringPreload |
The spring preload at the reference length or angle |
NXOpen.UF.MotionSpringDamper_Struct.SpringRefLength |
The reference length of the spring is used to calculate either the preload force on the spring or the free length. |
NXOpen.UF.MotionSpringDamper_Struct.SpringRefAngle |
The reference angle of the spring at zero displacement. |
NXOpen.UF.MotionSpringDamper_Struct.SpringInitLength |
The initial length of the spring at assembly position; used for spring defined on slide joint |
NXOpen.UF.MotionSpringDamper_Struct.DampingRate |
The linear damping rate of the damper. |