NXOpen.UF.Motion.SolverParameters Structure¶
NXOpen.UF.Motion.SolverParameters is an alias for NXOpen.UF.MotionSolverParameters_Struct
-
class
NXOpen.UF.
MotionSolverParameters_Struct
¶ Bases:
object
Refer to UF_MOTION_solver_parameters_s for documentation.
Fields
NXOpen.UF.MotionSolverParameters_Struct.Solver |
The solver to be used. |
NXOpen.UF.MotionSolverParameters_Struct.MaxStepSize |
The maximum allowed step size of the solver. |
NXOpen.UF.MotionSolverParameters_Struct.MaxSolverError |
The maximum integration error allowed by the solver. |
NXOpen.UF.MotionSolverParameters_Struct.MaxIntegratorIterations |
The maximum number of iterations allowed for the solver’s integrator to converge to the solution in a dynamic analysis.If the solver integrator has problems in converging during a dynamic analysis then increase this number |
NXOpen.UF.MotionSolverParameters_Struct.MaxKinematicsIterations |
The maximum number of iterations allowed for the solver to converge to the solution in a kinematic analysis.If the motion model has problems in converging during a kinematic analysis then increase this number |
NXOpen.UF.MotionSolverParameters_Struct.MaxStaticsIterations |
The maximum number of iterations allowed for the solver to converge to the solution in a static analysis. |
NXOpen.UF.MotionSolverParameters_Struct.UseMassProperties |
A flag to determine whether or not to use mass properties in the analysis. |