NXOpen.UF.Motion.PointOnSurfaceData Structure

NXOpen.UF.Motion.PointOnSurfaceData is an alias for NXOpen.UF.MotionPointOnSurfaceData_Struct

class NXOpen.UF.MotionPointOnSurfaceData_Struct

Bases: object

Refer to UF_MOTION_point_on_surface_data_s for documentation.

Fields

NXOpen.UF.MotionPointOnSurfaceData_Struct.PointOnSurfaceTag Tag of the created/edited entity
NXOpen.UF.MotionPointOnSurfaceData_Struct.PointTag The point tag of the point on surface constraint.
NXOpen.UF.MotionPointOnSurfaceData_Struct.PointLinkTag Optional: The user need not specify this data.
NXOpen.UF.MotionPointOnSurfaceData_Struct.NumFaceTags Number of face tags for the constraint
NXOpen.UF.MotionPointOnSurfaceData_Struct.FaceTags Group of faces that can be have a parameterized UV space.
NXOpen.UF.MotionPointOnSurfaceData_Struct.FaceLinkTag Optional: The user need not specify this data.
NXOpen.UF.MotionPointOnSurfaceData_Struct.DisplayScale This scale is used in UI for displaying the object
NXOpen.UF.MotionPointOnSurfaceData_Struct.EntityName A unique name for the object