NXOpen.UF.Motion.JointMotionInput Structure¶
NXOpen.UF.Motion.JointMotionInput is an alias for NXOpen.UF.MotionJointMotionInput_Struct
-
class
NXOpen.UF.
MotionJointMotionInput_Struct
¶ Bases:
object
Refer to UF_MOTION_joint_motion_input_s for documentation.
Fields
NXOpen.UF.MotionJointMotionInput_Struct.InputType |
The type of the motion input. |
NXOpen.UF.MotionJointMotionInput_Struct.Function |
The tag to the function. |
NXOpen.UF.MotionJointMotionInput_Struct.Displacement |
The constant displacement input. |
NXOpen.UF.MotionJointMotionInput_Struct.Velocity |
The constant velocity input. |
NXOpen.UF.MotionJointMotionInput_Struct.Acceleration |
The constant acceleration input. |
NXOpen.UF.MotionJointMotionInput_Struct.Amplitude |
The harmonic amplitude input. |
NXOpen.UF.MotionJointMotionInput_Struct.Frequency |
The harmonic frequency input. |
NXOpen.UF.MotionJointMotionInput_Struct.PhaseAngle |
The harmonic phase angle input. |
NXOpen.UF.MotionJointMotionInput_Struct.HarmDisp |
The harmonic offset displacement input. |