NXOpen.UF.Motion.JointCoupler Structure¶
NXOpen.UF.Motion.JointCoupler is an alias for NXOpen.UF.MotionJointCoupler_Struct
-
class
NXOpen.UF.
MotionJointCoupler_Struct
¶ Bases:
object
Refer to UF_MOTION_joint_coupler_s for documentation.
Fields
NXOpen.UF.MotionJointCoupler_Struct.Name |
The name of the joint coupler. |
NXOpen.UF.MotionJointCoupler_Struct.JtcType |
The type of the joint coupler. |
NXOpen.UF.MotionJointCoupler_Struct.Joint1 |
The first joint of the coupler. |
NXOpen.UF.MotionJointCoupler_Struct.Joint2 |
The second joint of the coupler. |
NXOpen.UF.MotionJointCoupler_Struct.Ratio |
The constraint ratio between the joints. |
NXOpen.UF.MotionJointCoupler_Struct.OriginTag |
The smart point that defines the origin of the contact point between the joints. |
NXOpen.UF.MotionJointCoupler_Struct.OrientationTag |
The orientation matrix that defines the orientation at the contact point between the two joints. |