NXOpen.UF.Motion.ContactParameters Structure¶
NXOpen.UF.Motion.ContactParameters is an alias for NXOpen.UF.MotionContactParameters_Struct
-
class
NXOpen.UF.
MotionContactParameters_Struct
¶ Bases:
object
Refer to UF_MOTION_contact_parameters_s for documentation.
Fields
NXOpen.UF.MotionContactParameters_Struct.ForceExponent |
The exponent of non-linear stiffness. |
NXOpen.UF.MotionContactParameters_Struct.MaterialDamping |
The linear damping rate relative to the penetration depth. |
NXOpen.UF.MotionContactParameters_Struct.PenetrationDepth |
The maximum overlap distance between contact objects. |
NXOpen.UF.MotionContactParameters_Struct.StaticFriction |
The coefficient of static friction at the static slip velocity. |
NXOpen.UF.MotionContactParameters_Struct.SlipVelocity |
The slip velocity of static friction where the static coefficient is maximum. |
NXOpen.UF.MotionContactParameters_Struct.DynamicFriction |
The coefficient of dynamic friction above the transition velocity. |
NXOpen.UF.MotionContactParameters_Struct.TransitionVelocity |
The dynamic transition velocity is the velocity at which the static friction effects disappear. |