NXOpen.UF.Modl.StycornerCrvOpt Structure¶
NXOpen.UF.Modl.StycornerCrvOpt is an alias for NXOpen.UF.ModlStycornerCrvOpt_Struct
-
class
NXOpen.UF.
ModlStycornerCrvOpt_Struct
¶ Bases:
object
Refer to UF_MODL_stycorner_crv_opt_s for documentation.
Fields
NXOpen.UF.ModlStycornerCrvOpt_Struct.ShapeControl |
***************************** 0: depth & skew, * 1: Tangent magnitude, * 2: Template * If shape_control is 2 (template), then there is no need to set the rest of the data structure ************************** |
NXOpen.UF.ModlStycornerCrvOpt_Struct.StartTagmag |
start tangent magnitude * must be set if shape_control is 1 (tangent magnitude), *********************************** |
NXOpen.UF.ModlStycornerCrvOpt_Struct.EndTagmag |
end tangent magnitude * must be set if shape_control is 1 (tangent magnitude), *********************************** |
NXOpen.UF.ModlStycornerCrvOpt_Struct.Depth |
depth of curve * must be set if shape_control is 0 (depth & skew), ******************************* |
NXOpen.UF.ModlStycornerCrvOpt_Struct.Skew |
skew of curve * must be set if shape_control is 0 (depth & skew), ******************************* |