NXOpen.UF.Modl.SolidPunchData Structure

NXOpen.UF.Modl.SolidPunchData is an alias for NXOpen.UF.ModlSolidPunchData_Struct

class NXOpen.UF.ModlSolidPunchData_Struct

Bases: object

Refer to UF_MODL_solid_punch_data_s for documentation.

Fields

NXOpen.UF.ModlSolidPunchData_Struct.Type punch type = 0; die type = 1
NXOpen.UF.ModlSolidPunchData_Struct.ThicknessOption 0 - infer,1 - use exp
NXOpen.UF.ModlSolidPunchData_Struct.Thickness
NXOpen.UF.ModlSolidPunchData_Struct.TargetFace Top target face
NXOpen.UF.ModlSolidPunchData_Struct.ToolBody punch or die tool
NXOpen.UF.ModlSolidPunchData_Struct.TargetCsysPt A point or CSYS eid.
NXOpen.UF.ModlSolidPunchData_Struct.ToolCsysPt A point or CSYS eid.
NXOpen.UF.ModlSolidPunchData_Struct.NPierceFaces Number of pierce faces
NXOpen.UF.ModlSolidPunchData_Struct.PierceFaces array of pierce faces
NXOpen.UF.ModlSolidPunchData_Struct.IsPtRequired Wether centroid is required or NOT