NXOpen.UF.Modl.SmholeData Structure¶
NXOpen.UF.Modl.SmholeData is an alias for NXOpen.UF.ModlSmholeData_Struct
-
class
NXOpen.UF.
ModlSmholeData_Struct
¶ Bases:
object
Refer to UF_MODL_smhole_data_s for documentation.
Fields
NXOpen.UF.ModlSmholeData_Struct.Diameter |
Diameter of SMHole |
NXOpen.UF.ModlSmholeData_Struct.Depth |
Depth of SMHole. |
NXOpen.UF.ModlSmholeData_Struct.TipAngle |
Tip angle of SMHole. |
NXOpen.UF.ModlSmholeData_Struct.Edge1 |
Tag of the firstoffset edge |
NXOpen.UF.ModlSmholeData_Struct.Offset1 |
Offset distance from first offset edge |
NXOpen.UF.ModlSmholeData_Struct.Edge2 |
Tag of the second offset edge |
NXOpen.UF.ModlSmholeData_Struct.Offset2 |
Offset distance from second offset edge |
NXOpen.UF.ModlSmholeData_Struct.HoleFace |
Tag of the face on which the SMHole will be placed |
NXOpen.UF.ModlSmholeData_Struct.ThruFace |
Tag of the facethrough which the Through SMHole will be created |
NXOpen.UF.ModlSmholeData_Struct.DatumAxis |
Tag of the datum axis used to determine the angle of the central axis of the SMHole. |
NXOpen.UF.ModlSmholeData_Struct.Method |
Method used to determine angle of central axis of the SMHole. |
NXOpen.UF.ModlSmholeData_Struct.VecDir |
Vector used to determine the angle of the central axis of the SMHole. |
NXOpen.UF.ModlSmholeData_Struct.Type |
Type of SMHole to be created. |