NXOpen.UF.Modl.SmcutoutData Structure¶
NXOpen.UF.Modl.SmcutoutData is an alias for NXOpen.UF.ModlSmcutoutData_Struct
-
class
NXOpen.UF.
ModlSmcutoutData_Struct
¶ Bases:
object
Refer to UF_MODL_smcutout_data_s for documentation.
Fields
NXOpen.UF.ModlSmcutoutData_Struct.PlacementFace |
Face to put cutout |
NXOpen.UF.ModlSmcutoutData_Struct.NCurves |
The number of curves in the curves array. |
NXOpen.UF.ModlSmcutoutData_Struct.Curves |
An array holding the tags to the curves that define the outline shape of the SMCutout |
NXOpen.UF.ModlSmcutoutData_Struct.ProjMethod |
The method used to determine the projection vector of the outline curves as well as the direction in which the cutout will be punched through the solid body. |
NXOpen.UF.ModlSmcutoutData_Struct.ProjVector |
Used when proj_method is UF_ALONG_VECTOR. |
NXOpen.UF.ModlSmcutoutData_Struct.DatumAxis |
Used when proj_method is UF_ALONG_DATUM_AXIS. |
NXOpen.UF.ModlSmcutoutData_Struct.FlipDiscardRegion |
When true the discard region is flipped from its normal calculation. |
NXOpen.UF.ModlSmcutoutData_Struct.Type |
Punch or through |
NXOpen.UF.ModlSmcutoutData_Struct.ThruFace |
Through face |