NXOpen.UF.Modl.Faces Structure

NXOpen.UF.Modl.Faces is an alias for NXOpen.UF.ModlFaces_Struct

class NXOpen.UF.ModlFaces_Struct

Bases: object

Refer to UF_MODL_faces_s for documentation.

Fields

NXOpen.UF.ModlFaces_Struct.NumberOfFaces Number of faces supplied in the following array.
NXOpen.UF.ModlFaces_Struct.Faces Array of faces to be used in the function.
NXOpen.UF.ModlFaces_Struct.FaceExtension Indication of how the faces should be extended if the function allows for face extension.