NXOpen.UF.Modl.EdgeBlendStopshortData Structure¶
NXOpen.UF.Modl.EdgeBlendStopshortData is an alias for NXOpen.UF.ModlEdgeBlendStopshortData_Struct
-
class
NXOpen.UF.
ModlEdgeBlendStopshortData_Struct
¶ Bases:
object
Refer to UF_MODL_edge_blend_stopshort_data_s for documentation.
Fields
NXOpen.UF.ModlEdgeBlendStopshortData_Struct.Edge |
The edge where the stopshort is defined |
NXOpen.UF.ModlEdgeBlendStopshortData_Struct.FromStart |
if true, then the stopshort is defined from the start of edge. Otherwise, it is defined from the end of edge. |
NXOpen.UF.ModlEdgeBlendStopshortData_Struct.Distance |
%Stopshort distance [0 - 100] |
NXOpen.UF.ModlEdgeBlendStopshortData_Struct.DistanceExp |
Expression TAG will only be set during Edit, User can edit the distance string to edit the new value |
NXOpen.UF.ModlEdgeBlendStopshortData_Struct.Status |
When adding Status = 1 and To remove Status = 0 |