NXOpen.UF.Modl.EdgeBlendMultData Structure¶
NXOpen.UF.Modl.EdgeBlendMultData is an alias for NXOpen.UF.ModlEdgeBlendMultData_Struct
-
class
NXOpen.UF.
ModlEdgeBlendMultData_Struct
¶ Bases:
object
Refer to UF_MODL_edge_blend_mult_data_s for documentation.
Fields
NXOpen.UF.ModlEdgeBlendMultData_Struct.BlendInstanced |
instanced blend |
NXOpen.UF.ModlEdgeBlendMultData_Struct.VrbTolerance |
tolerance of a variable blend |
NXOpen.UF.ModlEdgeBlendMultData_Struct.SmoothOverflow |
blend smooth overflow |
NXOpen.UF.ModlEdgeBlendMultData_Struct.CliffOverflow |
blend cliff overflow |
NXOpen.UF.ModlEdgeBlendMultData_Struct.NotchOverflow |
blend notch overflow |
NXOpen.UF.ModlEdgeBlendMultData_Struct.AllowTwistPatches |
Allow twist patches to be created. |
NXOpen.UF.ModlEdgeBlendMultData_Struct.SoftenVertices |
Y-Blend |
NXOpen.UF.ModlEdgeBlendMultData_Struct.NumSets |
number of blend sets to be blended |
NXOpen.UF.ModlEdgeBlendMultData_Struct.EdgeData |
Data of an edges/Blendset to be blended or an edge collector. |
NXOpen.UF.ModlEdgeBlendMultData_Struct.NumVarRad |
Number of points where variable radius is defined |
NXOpen.UF.ModlEdgeBlendMultData_Struct.VarEdges |
The edge on which the variable radius is defined |
NXOpen.UF.ModlEdgeBlendMultData_Struct.VarRadiusData |
Location of the edge and radius value for the variable radius |
NXOpen.UF.ModlEdgeBlendMultData_Struct.NumSetback |
Number of edges that have setbacks defined. |
NXOpen.UF.ModlEdgeBlendMultData_Struct.SetbackData |
Setback data on the edges. |
NXOpen.UF.ModlEdgeBlendMultData_Struct.NumStopshort |
Number of edges that have stopshorts defined. |
NXOpen.UF.ModlEdgeBlendMultData_Struct.StopshortData |
Stopshort data on the edges. |