NXOpen.UF.Modl.DimensionData Structure¶
NXOpen.UF.Modl.DimensionData is an alias for NXOpen.UF.ModlDimensionData_Struct
-
class
NXOpen.UF.
ModlDimensionData_Struct
¶ Bases:
object
Refer to UF_MODL_dimension_data_s for documentation.
Fields
NXOpen.UF.ModlDimensionData_Struct.Type |
Type of dimension - 0 - Parallel 1 - Diameter 2- angular 3- Radial 4 - RPO |
NXOpen.UF.ModlDimensionData_Struct.FeatureTag |
The tag of the feature associated with the dimension |
NXOpen.UF.ModlDimensionData_Struct.Value |
The value of the expression from which we create the dimension. |
NXOpen.UF.ModlDimensionData_Struct.FirstPoint |
The absolute coordinates of objects used to create the dimension. |
NXOpen.UF.ModlDimensionData_Struct.SecondPoint |
The second point necessary to create the parallel dimension. |
NXOpen.UF.ModlDimensionData_Struct.Origin |
Origin for the dimension placement in absolute coordinates. |
NXOpen.UF.ModlDimensionData_Struct.StartAngle |
Start angle for arc of radial dimensions in radians |
NXOpen.UF.ModlDimensionData_Struct.EndAngle |
End angle for arc of radial dimensions in radians |
NXOpen.UF.ModlDimensionData_Struct.CsysTag |
This is the coordinate system which defines the XY plane on which the dimension is created. |
NXOpen.UF.ModlDimensionData_Struct.DrfTxt |
Dimension text associated with the dimension. |
NXOpen.UF.ModlDimensionData_Struct.TopArray |
Topological information associated with the feature (such as faces or edges) which should be used to customize the dimension creation by the user. |
NXOpen.UF.ModlDimensionData_Struct.NumTopArray |
Number of topological entities returned |
NXOpen.UF.ModlDimensionData_Struct.FirstLine |
Used only when the dimension is angular, this is the first line to be created for the angular dimension. |
NXOpen.UF.ModlDimensionData_Struct.SecondLine |
Used only when the dimension is angular, this is the Second line to be created for the angular dimension. |