NXOpen.UF.Modl.DevchkEeInfo Structure

NXOpen.UF.Modl.DevchkEeInfo is an alias for NXOpen.UF.ModlDevchkEeInfo_Struct

class NXOpen.UF.ModlDevchkEeInfo_Struct

Bases: object

Refer to UF_MODL_devchk_ee_info_s for documentation.

Fields

NXOpen.UF.ModlDevchkEeInfo_Struct.DevType 0 - no deviation1 - step 2 - overlap 3 - gap
NXOpen.UF.ModlDevchkEeInfo_Struct.Face1Tag face tag on which edge_1_pnt lies
NXOpen.UF.ModlDevchkEeInfo_Struct.Edge1Pnt point on an edge of face_pairs[0] used for deviation checking
NXOpen.UF.ModlDevchkEeInfo_Struct.Norm1 face normal at edge_1_pnt
NXOpen.UF.ModlDevchkEeInfo_Struct.Face2Tag face tag on which edge_2_pnt lies
NXOpen.UF.ModlDevchkEeInfo_Struct.Edge2Pnt point on an edge of face_pairs[1], where the minimum deviation occured from edge_1_pnt
NXOpen.UF.ModlDevchkEeInfo_Struct.Norm2 face normal at edge_2_pnt
NXOpen.UF.ModlDevchkEeInfo_Struct.EdgeDist distance between edge_1_pnt and edge_2_pnt
NXOpen.UF.ModlDevchkEeInfo_Struct.NormAngle Angle between the face normals