NXOpen.UF.Modl.CompareOptions Structure¶
NXOpen.UF.Modl.CompareOptions is an alias for NXOpen.UF.ModlCompareOptions_Struct
-
class
NXOpen.UF.
ModlCompareOptions_Struct
¶ Bases:
object
Refer to UF_MODL_compare_options_s for documentation.
Fields
NXOpen.UF.ModlCompareOptions_Struct.Version |
Version number. |
NXOpen.UF.ModlCompareOptions_Struct.Tolerance |
Tolerance to be used to determine if two geometries can be considered coincident |
NXOpen.UF.ModlCompareOptions_Struct.Accuracy |
Accuracy setting for comparison |
NXOpen.UF.ModlCompareOptions_Struct.CompareFeatAndExp |
Whether to compare features and expressions. |
NXOpen.UF.ModlCompareOptions_Struct.IdenticalFaceRule |
Rule for classifying faces as identical |
NXOpen.UF.ModlCompareOptions_Struct.ContinueIfExamineGeomFails |
If any body fails in examine geometry, continue with comparison, results may not be meaningful |
NXOpen.UF.ModlCompareOptions_Struct.GenerateReport |
generate HTML report for the compared parts |