NXOpen.UF.Mfm Class¶
-
class
NXOpen.UF.
Mfm
¶ Bases:
object
Contains wrappers for all ‘UFMfm’ functions and data types.
Methods
NXOpen.UF.Mfm.AskFeatureType |
Refer to UF_MFM_ask_feature_type for documentation. |
NXOpen.UF.Mfm.SetFeatureName |
Refer to UF_MFM_set_feature_name for documentation. |
NXOpen.UF.Mfm.AskFeatureName |
Refer to UF_MFM_ask_feature_name for documentation. |
NXOpen.UF.Mfm.AskGeometryGroups |
Refer to UF_MFM_ask_geometry_groups for documentation. |
NXOpen.UF.Mfm.AskMachinedStatus |
Refer to UF_MFM_ask_machined_status for documentation. |
NXOpen.UF.Mfm.AskSourceType |
Refer to UF_MFM_ask_source_type for documentation. |
NXOpen.UF.Mfm.AskOverriddenStatus |
Refer to UF_MFM_ask_overridden_status for documentation. |
NXOpen.UF.Mfm.AskMachiningFeaturesOfPart |
Refer to UF_MFM_ask_machining_features_of_part for documentation. |
NXOpen.UF.Mfm.AskMachiningFeatureTypes |
Refer to UF_MFM_ask_machining_feature_types for documentation. |
NXOpen.UF.Mfm.AskMachiningFeaturesOfType |
Refer to UF_MFM_ask_machining_features_of_type for documentation. |
NXOpen.UF.Mfm.AskCandidateMachiningFeatureTypes |
Refer to UF_MFM_ask_candidate_machining_feature_types for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromModelingFeatures |
Refer to UF_MFM_create_machining_features_from_modeling_features for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromUserDefinedFeatures |
Refer to UF_MFM_create_machining_features_from_user_defined_features for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromTaggedPoints |
Refer to UF_MFM_create_machining_features_from_tagged_points for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromTaggedArcs |
Refer to UF_MFM_create_machining_features_from_tagged_arcs for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromTaggedEdges |
Refer to UF_MFM_create_machining_features_from_tagged_edges for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromTaggedFaces |
Refer to UF_MFM_create_machining_features_from_tagged_faces for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeaturesFromRecognizedFeatures |
Refer to UF_MFM_create_machining_features_from_recognized_features for documentation. |
NXOpen.UF.Mfm.DeleteMachiningFeatures |
Refer to UF_MFM_delete_machining_features for documentation. |
NXOpen.UF.Mfm.AskAttributes |
Refer to UF_MFM_ask_attributes for documentation. |
NXOpen.UF.Mfm.AskAttributeType |
Refer to UF_MFM_ask_attribute_type for documentation. |
NXOpen.UF.Mfm.AskLogicalValueOfAttribute |
Refer to UF_MFM_ask_logical_value_of_attribute for documentation. |
NXOpen.UF.Mfm.SetLogicalValueOfAttribute |
Refer to UF_MFM_set_logical_value_of_attribute for documentation. |
NXOpen.UF.Mfm.AskDoubleValueOfAttribute |
Refer to UF_MFM_ask_double_value_of_attribute for documentation. |
NXOpen.UF.Mfm.SetDoubleValueOfAttribute |
Refer to UF_MFM_set_double_value_of_attribute for documentation. |
NXOpen.UF.Mfm.AskIntegerValueOfAttribute |
Refer to UF_MFM_ask_integer_value_of_attribute for documentation. |
NXOpen.UF.Mfm.SetIntegerValueOfAttribute |
Refer to UF_MFM_set_integer_value_of_attribute for documentation. |
NXOpen.UF.Mfm.AskStringValueOfAttribute |
Refer to UF_MFM_ask_string_value_of_attribute for documentation. |
NXOpen.UF.Mfm.SetStringValueOfAttribute |
Refer to UF_MFM_set_string_value_of_attribute for documentation. |
NXOpen.UF.Mfm.HasSelectedFeaList |
Refer to UF_MFM_has_selected_fea_list for documentation. |
NXOpen.UF.Mfm.CleanSelectedFeaList |
Refer to UF_MFM_clean_selected_fea_list for documentation. |
NXOpen.UF.Mfm.SetSelectedFeaList |
Refer to UF_MFM_set_selected_fea_list for documentation. |
NXOpen.UF.Mfm.AskSelectedFeaList |
Refer to UF_MFM_ask_selected_fea_list for documentation. |
NXOpen.UF.Mfm.SetIntUgAttribute |
Refer to UF_MFM_set_int_ug_attribute for documentation. |
NXOpen.UF.Mfm.SetDoubleUgAttribute |
Refer to UF_MFM_set_double_ug_attribute for documentation. |
NXOpen.UF.Mfm.SetStringUgAttribute |
Refer to UF_MFM_set_string_ug_attribute for documentation. |
NXOpen.UF.Mfm.AskListOfFaces |
Refer to UF_MFM_ask_list_of_faces for documentation. |
NXOpen.UF.Mfm.RecognizeHoles |
Refer to UF_MFM_recognize_holes for documentation. |
NXOpen.UF.Mfm.CreateMachiningFeature |
Refer to UF_MFM_create_machining_feature for documentation. |
Enumerations
NXOpen.UF.Mfm.AttrValueType Enumeration |
NXOpen.UF.Mfm.MachinedStatus Enumeration |
NXOpen.UF.Mfm.SourceType Enumeration |
Structures
NXOpen.UF.Mfm.RecognizeOptions Structure |