NXOpen.UF.Gdt.ToleranceZone Structure¶
NXOpen.UF.Gdt.ToleranceZone is an alias for NXOpen.UF.GdtToleranceZone_Struct
-
class
NXOpen.UF.
GdtToleranceZone_Struct
¶ Bases:
object
Refer to UF_GDT_tolerance_zone_s for documentation.
Fields
NXOpen.UF.GdtToleranceZone_Struct.ZoneShape |
Shape of the tolerance zone |
NXOpen.UF.GdtToleranceZone_Struct.PlanarRef |
Object that defines zone when it is not defined by the face set |
NXOpen.UF.GdtToleranceZone_Struct.Expression |
Expression for the tolerance value |
NXOpen.UF.GdtToleranceZone_Struct.Value |
Actual value of the tolerance |
NXOpen.UF.GdtToleranceZone_Struct.DecimalFormat |
Number of digits right of decimal |
NXOpen.UF.GdtToleranceZone_Struct.MaterialModifier |
Material modifier |