NXOpen.UF.Gdt.ThreadData Structure

NXOpen.UF.Gdt.ThreadData is an alias for NXOpen.UF.GdtThreadData_Struct

class NXOpen.UF.GdtThreadData_Struct

Bases: object

Refer to UF_GDT_thread_data_s for documentation.

Fields

NXOpen.UF.GdtThreadData_Struct.PitchDiaGrade Tolerance grade based on pitch diameter
NXOpen.UF.GdtThreadData_Struct.PitchDiaDeviation Deviation based on pitch diameter
NXOpen.UF.GdtThreadData_Struct.Grade Tolerance grade based on major/minor diameter
NXOpen.UF.GdtThreadData_Struct.Deviation Deviation based on major/minor diameter
NXOpen.UF.GdtThreadData_Struct.ThreadClass Thread class for ANSI non-metric threads