NXOpen.UF.Gdt.TargetUdefArea Structure¶
NXOpen.UF.Gdt.TargetUdefArea is an alias for NXOpen.UF.GdtTargetUdefArea_Struct
-
class
NXOpen.UF.
GdtTargetUdefArea_Struct
¶ Bases:
object
Refer to UF_GDT_target_udef_area_s for documentation.
Fields
NXOpen.UF.GdtTargetUdefArea_Struct.DatumFeature |
This corresponds to the tag of the parent datum feature the target is to be applied to. |
NXOpen.UF.GdtTargetUdefArea_Struct.TargetIndex |
Datum target index to assign to new datum targets. |
NXOpen.UF.GdtTargetUdefArea_Struct.Curves |
Array of curves defining the user defined area. |
NXOpen.UF.GdtTargetUdefArea_Struct.NumCurves |
Number of curves in the array |
NXOpen.UF.GdtTargetUdefArea_Struct.IsPlanar |
Is this a planar datum target area? * Creation and Query routines only. |
NXOpen.UF.GdtTargetUdefArea_Struct.NpData |