NXOpen.UF.Gdt.TargetDiaArea Structure

NXOpen.UF.Gdt.TargetDiaArea is an alias for NXOpen.UF.GdtTargetDiaArea_Struct

class NXOpen.UF.GdtTargetDiaArea_Struct

Bases: object

Refer to UF_GDT_target_dia_area_s for documentation.

Fields

NXOpen.UF.GdtTargetDiaArea_Struct.DatumFeature The tag of the parent datum feature the target is to be applied to.
NXOpen.UF.GdtTargetDiaArea_Struct.TargetIndex Datum target index to assign to new datum targets.
NXOpen.UF.GdtTargetDiaArea_Struct.Point Identifier of smart point locating the center * of the target.
NXOpen.UF.GdtTargetDiaArea_Struct.Diameter Size of the outer datum target area diameter
NXOpen.UF.GdtTargetDiaArea_Struct.InnerDia Size of the inner diameter for annular areas
NXOpen.UF.GdtTargetDiaArea_Struct.IsPlanar Is this a planar datum target area? * Creation and Query routines only.
NXOpen.UF.GdtTargetDiaArea_Struct.Orientation Orientation of area relative to surface.
NXOpen.UF.GdtTargetDiaArea_Struct.Location Absolute position of target (output only)