NXOpen.UF.Gdt.TargetCylArea Structure¶
NXOpen.UF.Gdt.TargetCylArea is an alias for NXOpen.UF.GdtTargetCylArea_Struct
-
class
NXOpen.UF.
GdtTargetCylArea_Struct
¶ Bases:
object
Refer to UF_GDT_target_cyl_area_s for documentation.
Fields
NXOpen.UF.GdtTargetCylArea_Struct.DatumFeature |
Parent datum feature |
NXOpen.UF.GdtTargetCylArea_Struct.TargetIndex |
Unique index of datum target |
NXOpen.UF.GdtTargetCylArea_Struct.StartPoint |
Identifier of start point locating * the start point of the target |
NXOpen.UF.GdtTargetCylArea_Struct.EndPoint |
Identifier of end point locating * the end point of the target |
NXOpen.UF.GdtTargetCylArea_Struct.StartLocation |
Absolute position of start point * (output only) |
NXOpen.UF.GdtTargetCylArea_Struct.EndLocation |
Absolute position of end point * (output only) |