NXOpen.UF.Gdt.MultipleDatum Structure¶
NXOpen.UF.Gdt.MultipleDatum is an alias for NXOpen.UF.GdtMultipleDatum_Struct
-
class
NXOpen.UF.
GdtMultipleDatum_Struct
¶ Bases:
object
Refer to UF_GDT_multiple_datum_s for documentation.
Fields
NXOpen.UF.GdtMultipleDatum_Struct.NumDatums |
Number of datum identifiers that define the multiple datum |
NXOpen.UF.GdtMultipleDatum_Struct.DatumFeatures |
Array of datum features referenced by the geometric tolerance |
NXOpen.UF.GdtMultipleDatum_Struct.DefFeat |
Where multiple feature types are possible a defining model feature for the multiple datum |