NXOpen.UF.Gdt.DatumTargetPoint Structure

NXOpen.UF.Gdt.DatumTargetPoint is an alias for NXOpen.UF.GdtDatumTargetPoint_Struct

class NXOpen.UF.GdtDatumTargetPoint_Struct

Bases: object

Refer to UF_GDT_datum_target_point_s for documentation.

Fields

NXOpen.UF.GdtDatumTargetPoint_Struct.PointOnSurface The identifier of the point which defines the target point
NXOpen.UF.GdtDatumTargetPoint_Struct.PointData The actual position of the target on their referencing plane
NXOpen.UF.GdtDatumTargetPoint_Struct.DatumFeature The identifier of the datum feature that the target constrains
NXOpen.UF.GdtDatumTargetPoint_Struct.TargetIndex The identifier of the target point