NXOpen.UF.Fam.IntentData Structure¶
NXOpen.UF.Fam.IntentData is an alias for NXOpen.UF.FamIntentData_Struct
-
class
NXOpen.UF.
FamIntentData_Struct
¶ Bases:
object
Refer to UF_FAM_intent_data_s for documentation.
Fields
NXOpen.UF.FamIntentData_Struct.Family |
The family involved in the intent. |
NXOpen.UF.FamIntentData_Struct.MemberIndex |
Desired family member…used only when attribute_count equals zero. |
NXOpen.UF.FamIntentData_Struct.AttributeCount |
The number of family attributes involved in the intent |
NXOpen.UF.FamIntentData_Struct.Attributes |
An array of attribute tags. |
NXOpen.UF.FamIntentData_Struct.MatchCriteria |
The match criteria for this intent…one per attribute. |
NXOpen.UF.FamIntentData_Struct.Name |
The name of the intent |