NXOpen.UF.Fam.ClassData Structure

NXOpen.UF.Fam.ClassData is an alias for NXOpen.UF.FamClassData_Struct

class NXOpen.UF.FamClassData_Struct

Bases: object

Refer to UF_FAM_class_data_s for documentation.

Fields

NXOpen.UF.FamClassData_Struct.Subtype A flag indicating the type of attributes in this class.
NXOpen.UF.FamClassData_Struct.AttributeCount The number of attributes in this class
NXOpen.UF.FamClassData_Struct.AttributeData An array of family attribute structures(see below).
NXOpen.UF.FamClassData_Struct.Name The name of the attribute class.