NXOpen.UF.Eval.Parabola Structure¶
NXOpen.UF.Eval.Parabola is an alias for NXOpen.UF.EvalParabola_Struct
-
class
NXOpen.UF.
EvalParabola_Struct
¶ Bases:
object
Refer to UF_EVAL_parabola_s for documentation.
Fields
NXOpen.UF.EvalParabola_Struct.Limits |
Curve limits: [0] = min [1] = max |
NXOpen.UF.EvalParabola_Struct.K1 |
Conic coefficient |
NXOpen.UF.EvalParabola_Struct.Center |
|
NXOpen.UF.EvalParabola_Struct.XAxis |
Unit direction vector of the x axis (ABS) |
NXOpen.UF.EvalParabola_Struct.YAxis |
Unit direction vector of the y axis (ABS) |