NXOpen.UF.Eval.Hyperbola Structure¶
NXOpen.UF.Eval.Hyperbola is an alias for NXOpen.UF.EvalHyperbola_Struct
-
class
NXOpen.UF.
EvalHyperbola_Struct
¶ Bases:
object
Refer to UF_EVAL_hyperbola_s for documentation.
Fields
NXOpen.UF.EvalHyperbola_Struct.Limits |
Curve limits: [0] = min [1] = max |
NXOpen.UF.EvalHyperbola_Struct.K1 |
First coefficient for evaluating hyperbola |
NXOpen.UF.EvalHyperbola_Struct.K2 |
Second coefficient for evaluating hyperbola Note that the limits and k1,k2 are values used for efficient evaluation of the hyperbola and are not the same as the start/end parameters and k1,k2 of UF_CURVE_ask_conic_data. |
NXOpen.UF.EvalHyperbola_Struct.Center |
|
NXOpen.UF.EvalHyperbola_Struct.XAxis |
Unit direction vector of the x axis (ABS) |
NXOpen.UF.EvalHyperbola_Struct.YAxis |
Unit direction vector of the y axis (ABS) |