NXOpen.UF.Eval.Ellipse Structure

NXOpen.UF.Eval.Ellipse is an alias for NXOpen.UF.EvalEllipse_Struct

class NXOpen.UF.EvalEllipse_Struct

Bases: object

Refer to UF_EVAL_ellipse_s for documentation.

Fields

NXOpen.UF.EvalEllipse_Struct.IsPeriodic Is the curve periodic or not?
NXOpen.UF.EvalEllipse_Struct.Limits Curve limits: [0] = min; [1] = max
NXOpen.UF.EvalEllipse_Struct.Minor Minor radius
NXOpen.UF.EvalEllipse_Struct.Major Major radius
NXOpen.UF.EvalEllipse_Struct.Center
NXOpen.UF.EvalEllipse_Struct.XAxis Unit direction vector of the x axis (ABS)
NXOpen.UF.EvalEllipse_Struct.YAxis Unit direction vector of the y axis (ABS)