NXOpen.UF.Eval.Arc Structure¶
NXOpen.UF.Eval.Arc is an alias for NXOpen.UF.EvalArc_Struct
-
class
NXOpen.UF.
EvalArc_Struct
¶ Bases:
object
Refer to UF_EVAL_arc_s for documentation.
Fields
NXOpen.UF.EvalArc_Struct.IsPeriodic |
Is the curve periodic or not? |
NXOpen.UF.EvalArc_Struct.Limits |
Curve limits (in radians): [0] = min; [1] = max |
NXOpen.UF.EvalArc_Struct.Radius |
|
NXOpen.UF.EvalArc_Struct.Center |
|
NXOpen.UF.EvalArc_Struct.XAxis |
Unit direction vector of the x axis (ABS) |
NXOpen.UF.EvalArc_Struct.YAxis |
Unit direction vector of the y axis (ABS) |