NXOpen.UF.Drf.WeldSymbols Structure¶
NXOpen.UF.Drf.WeldSymbols is an alias for NXOpen.UF.DrfWeldSymbols_Struct
-
class
NXOpen.UF.
DrfWeldSymbols_Struct
¶ Bases:
object
Refer to UF_DRF_weld_symbols_s for documentation.
Fields
NXOpen.UF.DrfWeldSymbols_Struct.SymInfoTop |
symbols info for top |
NXOpen.UF.DrfWeldSymbols_Struct.SymInfoBottom |
symbols info forbottom |
NXOpen.UF.DrfWeldSymbols_Struct.Extension |
extension |
NXOpen.UF.DrfWeldSymbols_Struct.IdentLineType |
type of identification line |
NXOpen.UF.DrfWeldSymbols_Struct.PeripheralFlag |
variable indicating whether allround symbol is required or not. If peripheral_flag = 0, then no allround symbol. If peripheral_flag = 1, then allround symbol is required |
NXOpen.UF.DrfWeldSymbols_Struct.FieldFlag |
value for field flag field_flag = 0 for weld at site; field_flag= 1 for weld at field |
NXOpen.UF.DrfWeldSymbols_Struct.StaggeredFlag |
indicates whether weld is staggered or not. staggered_flag = 0 for non-staggered welds; staggered_flag = 1 for staggered welds |
NXOpen.UF.DrfWeldSymbols_Struct.CenterFlag |
indicates whether weld to be centered with respect to reference line. Applicable for spot and seam welds only. center_flag = 0 => donot center; center_flag = 1 => center |
NXOpen.UF.DrfWeldSymbols_Struct.NumLines |
number of lines of reference text |
NXOpen.UF.DrfWeldSymbols_Struct.SymbolStandard |
standard for the weld symbol. Has to be one among the following : ANSI, ISO, DIN, JIS. |
NXOpen.UF.DrfWeldSymbols_Struct.ReferenceText |
multi line reference text |
NXOpen.UF.DrfWeldSymbols_Struct.ScaleFactor |
scale factor to be used for creating the welding symbol |