NXOpen.UF.Drf.ObjectAssocData Structure¶
NXOpen.UF.Drf.ObjectAssocData is an alias for NXOpen.UF.DrfObjectAssocData_Struct
-
class
NXOpen.UF.
DrfObjectAssocData_Struct
¶ Bases:
object
Refer to UF_DRF_object_assoc_data_s for documentation.
Fields
NXOpen.UF.DrfObjectAssocData_Struct.AssocObject1 |
Tag of first referenced object |
NXOpen.UF.DrfObjectAssocData_Struct.AssocObject2 |
Tag of second referenced object (for * intersections) |
NXOpen.UF.DrfObjectAssocData_Struct.ObjectView |
Drawing or drafting member view of the * associatied objects. |
NXOpen.UF.DrfObjectAssocData_Struct.PointType |
Point / Line options for associativities |
NXOpen.UF.DrfObjectAssocData_Struct.LineType |
Line option data |
NXOpen.UF.DrfObjectAssocData_Struct.BasePt1 |
Used for line options with 1 point * (in absolute of work view) |
NXOpen.UF.DrfObjectAssocData_Struct.BasePt2 |
Used for line options with 2 points * (in absolute of work view) |
NXOpen.UF.DrfObjectAssocData_Struct.EnteredAngle |
Used for entered angle line method * (in radians) |
NXOpen.UF.DrfObjectAssocData_Struct.AssocPoint |
Associated position or reference point of the associativity * in absolute coordinates. |