NXOpen.UF.Drf.LineObject Structure¶
NXOpen.UF.Drf.LineObject is an alias for NXOpen.UF.DrfLineObject_Struct
-
class
NXOpen.UF.
DrfLineObject_Struct
¶ Bases:
object
Refer to UF_DRF_line_object_s for documentation.
Fields
NXOpen.UF.DrfLineObject_Struct.LineAssocType |
line associativity type as defined by UF_DRF_assoc_line_type_t, UF_DRF_EXISTING_LINE UF_DRF_TWO_POINTS UF_DRF_DWG_LINE |
NXOpen.UF.DrfLineObject_Struct.Object1 |
For UF_DRF_EXISTING_LINE this is the UF_DRF_object_t that contains the line definition as defined by UF_DRF_object_t. |
NXOpen.UF.DrfLineObject_Struct.PointObject2 |
For UF_DRF_EXISTING_LINE this is unused. |