NXOpen.UF.Drf.LetteringPreferences Structure¶
NXOpen.UF.Drf.LetteringPreferences is an alias for NXOpen.UF.DrfLetteringPreferences_Struct
-
class
NXOpen.UF.
DrfLetteringPreferences_Struct
¶ Bases:
object
Refer to UF_DRF_lettering_preferences_s for documentation.
Fields
NXOpen.UF.DrfLetteringPreferences_Struct.AlignPosition |
one of nine site locations in the text rectangle used to place the text |
NXOpen.UF.DrfLetteringPreferences_Struct.HorizTextJust |
horizontal textjustification |
NXOpen.UF.DrfLetteringPreferences_Struct.GdtFrameHeightFactor |
GD&T frame height factor |
NXOpen.UF.DrfLetteringPreferences_Struct.Angle |
angle for general text |
NXOpen.UF.DrfLetteringPreferences_Struct.DimensionText |
lettering preferences for dimension text |
NXOpen.UF.DrfLetteringPreferences_Struct.AppendedText |
lettering preferences for appended text |
NXOpen.UF.DrfLetteringPreferences_Struct.ToleranceText |
lettering preferences for tolerance text |
NXOpen.UF.DrfLetteringPreferences_Struct.GeneralText |
lettering preferences for drafting aid text |
NXOpen.UF.DrfLetteringPreferences_Struct.DimDimLineSpaceFactor |
this controls spacing between bottom most piece of text on the dimension and the dimension line when text orientation is UF_DRF_DIMENSION_TEXT_OVER_DIMENSION_LINE. This factor is applied to the dimension text character size to determine the spacing |
NXOpen.UF.DrfLetteringPreferences_Struct.DimAppTextSpaceFactor |
controls spacing between before appended text and next piece of dimension text to its right, and spacing between the after appended text and next piece of dimension text to its left. This factor is applied to the appended text character size to determine the spacing |
NXOpen.UF.DrfLetteringPreferences_Struct.DimTolTextSpaceFactor |
controls spacing between dimension main text and after tolerance text. this factor is applied to the tolerance text character size to determine the spacing |