NXOpen.UF.Drf.LeaderInfo Structure¶
NXOpen.UF.Drf.LeaderInfo is an alias for NXOpen.UF.DrfLeaderInfo_Struct
-
class
NXOpen.UF.
DrfLeaderInfo_Struct
¶ Bases:
object
Refer to UF_DRF_leader_info_s for documentation.
Fields
NXOpen.UF.DrfLeaderInfo_Struct.LeaderAttachType |
Each leader may have up to 7 intermediate points. |
NXOpen.UF.DrfLeaderInfo_Struct.NumLinebks |
Number of graphical line elements used to represent the leader in the display. |
NXOpen.UF.DrfLeaderInfo_Struct.LeaderPnts |
Array of structures, one for each of the num_linebks line elements. |
NXOpen.UF.DrfLeaderInfo_Struct.NumAssocObjs |
number of associated objects |
NXOpen.UF.DrfLeaderInfo_Struct.AssocObjs |
Array of leader associated objects, one structure for each of the num_assoc_o bjs objects. |