NXOpen.UF.Drf.ImageData Structure¶
NXOpen.UF.Drf.ImageData is an alias for NXOpen.UF.DrfImageData_Struct
-
class
NXOpen.UF.
DrfImageData_Struct
¶ Bases:
object
Refer to UF_DRF_image_data_s for documentation.
Fields
NXOpen.UF.DrfImageData_Struct.ImageName |
The name of image in the part |
NXOpen.UF.DrfImageData_Struct.DrawingSheet |
The drawing sheet on which to create the * image or NULL_TAG to create the image on * the current drawing sheet. |
NXOpen.UF.DrfImageData_Struct.AspectRatioLocked |
TRUE if the image’s aspect ratio * cannot be changed |
NXOpen.UF.DrfImageData_Struct.Width |
The width of the image in drawing * sheet units * 0.0 to use original image length |
NXOpen.UF.DrfImageData_Struct.Height |
The height of the image in drawing * sheet units * 0.0 to use original image height |
NXOpen.UF.DrfImageData_Struct.AlignmentPosition |
The location to use when aligning the * image to another object |
NXOpen.UF.DrfImageData_Struct.Origin |
Point in drawing sheet units defining the * image origin which is located at the * image alignment_position |
NXOpen.UF.DrfImageData_Struct.WidthDir |
Vector defining the direction in which * the image width is displayed * Currently, images can only be rotated in * 90-degree increments so this vector will * always be parallel or perpendicular to * the drawing sheet’s X-axis |
NXOpen.UF.DrfImageData_Struct.HeightDir |
Vector defining the direction in which * the image height is displayed * Currently, images can only be rotated in * 90-degree increments so this vector will * always be parallel or perpendicular to * the drawing sheet’s Y-axis |