NXOpen.UF.Drf.GdtLeaderData Structure

NXOpen.UF.Drf.GdtLeaderData is an alias for NXOpen.UF.DrfGdtLeaderData_Struct

class NXOpen.UF.DrfGdtLeaderData_Struct

Bases: object

Refer to UF_DRF_gdt_leader_data_s for documentation.

Fields

NXOpen.UF.DrfGdtLeaderData_Struct.Object This is the tag of the associated object.
NXOpen.UF.DrfGdtLeaderData_Struct.View This is the tag of the member view of the object_tag entity.
NXOpen.UF.DrfGdtLeaderData_Struct.Point This 3D point is the location of the terminator (or arrow) of the leader.
NXOpen.UF.DrfGdtLeaderData_Struct.IntermediatePoints These are the intermediate points, if any, between the stub and the terminator of the leader.