NXOpen.UF.Drf.DiameterRadiusPreferences Structure¶
NXOpen.UF.Drf.DiameterRadiusPreferences is an alias for NXOpen.UF.DrfDiameterRadiusPreferences_Struct
-
class
NXOpen.UF.
DrfDiameterRadiusPreferences_Struct
¶ Bases:
object
Refer to UF_DRF_diameter_radius_preferences_s for documentation.
Fields
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.DiameterSymbolType |
standard diameter symbol or user-defined |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.DiameterSymbol |
text for user-defined diameter symbol |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.RadiusSymbolType |
standard radius symbol or user-defined |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.RadiusSymbol |
text for user-defined radius symbol |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.DiameterRadiusPlacement |
placement of diameter/radius symbol relative to dimension text |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.TextAboveLeader |
if option is set to anything other than UF_DRF_NO_TEXT_ABOVE_LEADER, then dimension text will be displayed above the leader stub with the stub extended to the maximum length of the dimension text. used with dimension text orientations of UF_DRF_TEXT_DIMENSION_HORIZONTAL and UF_DRF_TEXT_DIMENSION_BY_ANGLE. for UF_DRF_NO_TEXT_ABOVE_LEADER, the dimension text displays next to the leader stub |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.SymbolToDimensionTextDistance |
distance between radius/ diameter symbol and dimension text in character spaces |
NXOpen.UF.DrfDiameterRadiusPreferences_Struct.FoldedRadiusAngle |
angle of the fold for folded radius dimensions |