NXOpen.UF.Drf.CustomSymbol Structure

NXOpen.UF.Drf.CustomSymbol is an alias for NXOpen.UF.DrfCustomSymbol_Struct

class NXOpen.UF.DrfCustomSymbol_Struct

Bases: object

Refer to UF_DRF_custom_symbol_s for documentation.

Fields

NXOpen.UF.DrfCustomSymbol_Struct.Geometry Tags of lines, arcs, splines, crosshatch, and area fill for symbol definition
NXOpen.UF.DrfCustomSymbol_Struct.NumGeometry Number of tags in the curves array above.
NXOpen.UF.DrfCustomSymbol_Struct.Text Array of symbol text structures for symbol definition.
NXOpen.UF.DrfCustomSymbol_Struct.NumText Number of text structures in the text array.
NXOpen.UF.DrfCustomSymbol_Struct.AnchorPoint Tag of the symbol’s anchor point.
NXOpen.UF.DrfCustomSymbol_Struct.Connections Array of tags for the symbol’s leader connect points.
NXOpen.UF.DrfCustomSymbol_Struct.NumConnections Number of leader connection points.
NXOpen.UF.DrfCustomSymbol_Struct.Leader Pointer to information about the leader
NXOpen.UF.DrfCustomSymbol_Struct.Angle The angle of the symbol with respect to the WCS X-axis
NXOpen.UF.DrfCustomSymbol_Struct.Scale The scale of the symbol with respect to the size of the original geometry
NXOpen.UF.DrfCustomSymbol_Struct.Origin The origin of the symbol in absolute coordinates.